请问DLP2010NIR可以用DLP4500NIR代替吗?或者其他的也可以
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
请问DLP2010NIR可以用DLP4500NIR代替吗?或者其他的也可以
DLP2010NIR和DLP4500NIR是不同定位的产品,根据应用领域的不同,可以有不同选择:
参考:http://www.ti.com/tool/dlpnirnanoevm
| Mobile Sensing EVM | High Performance EVM | |
| Key Features | DLP NIRscan Nano | DLP NIRscan |
| Evaluation Module (EVM) Usage | Battery | Benchtop/Portable |
| Featured Digital Micromirror Device | DLP2010NIR | DLP4500NIR |
|
Micromirror Array Size (pixels) |
854 x 480 | 912 x 1140 |
| Micromirror Pixel Pitch (µm) | 5.4 | 7.6 |
| Micromirror Tilt Angle (degrees) | +/-17 | +/-12 |
| EVM Wavelength Range | 900-1700nm | 1350-2490nm |
| EVM Spectral Resolution | 10nm | 12nm |
| EVM Max Scan Speed (kHz) | 2.88 | 4 |
| EVM Signal-to-Noise Ratio |
6,000:1 (reflective head) |
30,000: 1 (transmissive head) |