This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

车规级HUD,EVM采购低成本

Other Parts Discussed in Thread: DLP3030-Q1

hello

我想采购一款车规级HUD的EVM进行功能评估,看看是否符合我们的要求。

我看了一下DLP3030-Q1,这个是最新的产品,虚拟成像达到了20m。

所以我想测试一下达到20的效果是什么样的,是否能覆盖整个挡风玻璃。 请问我购置哪款EVM可以进行评估?价格经济点的。

另外,对于挡风玻璃的材质是否有要求?我拿到EVM的时候,是否可以用普通的玻璃进行测试。

谢谢