DLPC6401 数据手册上说可以接受 YUV信号,请问硬件怎么接?分别对应哪些pin~ 谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好!
感谢您选择TI的产品,YUV信号使用的是PARALLEL VIDEO AND GRAPHICS INPUT接口,datasheet Page5
http://www.ti.com/lit/ds/symlink/dlpc6401.pdf
可以通过I2C命令将其配置成YUV格式,编程手册Page 24
http://www.ti.com/lit/ug/dlpu012/dlpu012.pdf
您也可以参考原理图
http://www.ti.com/lit/df/tidrhu9/tidrhu9.pdf
希望这个回复可以帮助到您
YUV可以20BITS或30BITS.
也可以BT656, 8BITS或10BITS.
Digital video output of R/Cr, ROUT [9] is MSB.
Digital video output of G/Y, GOUT [9] is MSB.
Digital video output of B/Cb, BOUT [9] is MSB.
如果使用YCbCr,软件需要配置的.