Dear ,
9500 dmd 在做block RST 的时候,可以边加载数据,边RST。那么,DMD在加载数据的时候,是否可以执行float 操作呢?
以上,
感谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear ,
9500 dmd 在做block RST 的时候,可以边加载数据,边RST。那么,DMD在加载数据的时候,是否可以执行float 操作呢?
以上,
感谢!
参考http://www.ti.com/lit/ds/symlink/dlpc410.pdf
第38页关于FLOAT操作.
和block reset不一样, reset后DMD立即显示.
FLOAT后DMD就就释放为FLAT.
While RST_ACTIVE is high, and for 8 μs after, the data for the block(s) being issued a Mirror Clocking Pulse
should not be changed to allow for the settling required for the mirrors to become stable.
It is possible to load other blocks while the block previously issued a Mirror Clocking Pulse is settling. Figure 13
shows a single block load, Mirror Clocking Pulse and reload sequence with the light gray areas indicating mirror
settling time.
It is best to issue a float command to avoid leaving a static image on the DMD for extended periods of time. A
mirror float sequence begins by asserting the proper BLK_MD and BLK_AD as described in Table 9. During the
following row cycle, the DMD releases the tension under each mirror so that all mirrors are in a relatively flat
position. The float operation takes approximately 3 μs to complete, during which time RST_ACTIVE is asserted.
FLOAT目的何在? TI的目的是:
It is best to issue a float command to avoid leaving a static image on the DMD for extended periods of time.
During the following row cycle, the DMD releases the tension under each mirror so that all mirrors are in a relatively flat
position. The float operation takes approximately 3 μs to complete, during which time RST_ACTIVE is asserted.