1.我们现在使用DLP4500的TRIG_OUT_1信号对外触发
2.我们要求DLP每投影1幅图片就会向外输出一个脉冲方波信号,也就是我如果使用20幅1bit的图片,我需要依次投射出20个对外脉冲方波信号
3.实际情况是我使用GUI软件的pattern sequence start/stop/pause进行先期测试的时候,其输出脉冲可以满足我的要求,即每投一副图片就可以就输出一个脉冲(用示波器观察)
4.但是当我将这个配置连同图片一同firmware update到DLP系统后,我下次重启上电DLP设备而不连GUI软件让其自己自动循环投影图片,那这个时候我们发现其是投完一个图片序列(20幅图片)才会输出一个脉冲,这个与测试时TRIG_OUT_1的信号完全不一样,请问如何解决该问题,谢谢