能帮我解释下dlpdlcr2000evm的工作原理吗?比如dlp2607、DLPA1000、DLP2000他们之间是怎么工作的?还有就是这个dlpdlcr2000evm是否需要烧录固件,如果需要烧录固件,官方会提供固件的下载么?谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
能帮我解释下dlpdlcr2000evm的工作原理吗?比如dlp2607、DLPA1000、DLP2000他们之间是怎么工作的?还有就是这个dlpdlcr2000evm是否需要烧录固件,如果需要烧录固件,官方会提供固件的下载么?谢谢!
您好!
感谢您关注TI的DLP产品。
dlpdlcr2000evm上有flash,用于存放DLPC2607的固件,是已经烧录好的,不需要客户自己烧录。
其次DLP2000是DMD,上面有很多的微镜,可以用于调整光路,DLPC2607是DMD的控制器,用于接收视频信号并发送给DMD,DLPA1000是电源芯片,用于控制DLP系统供电以及复位等。详细的DLP系统工作原理请参考:
http://www.ti.com/lit/wp/dlpa059c/dlpa059c.pdf

了解更多DLP2010EVM的资料,请参考:

TI.com上提供了该EVM的原理图/PCB/BOM/测试文件/用户手册/数据手册等等全套资料。
希望这个回答可以帮助到您。