hi,
我在ubuntu上面编译3dtof/voxelsdk的sdk的时候出现以下问题,尝试了很多方法不知道怎么解决这个问题,你们能够提供一些帮助吗?
还有我现在有一个opt8241的开发板,我想在我的arm开发板上面后去opt8241的数据,有没有什么demo可以去参考的?若有的话麻烦发一个链接过来看下 谢谢!
[ 62%] Building CXX object TI3DToF/CMakeFiles/ti3dtof.dir/VoxelProgrammerBase.cpp.o
/home/jason/TI-tof/libvoxel/voxelsdk/Voxel/SWIG/../Device.h:63: Error: Syntax error in input(3).
make[2]: *** [lib/python2.7/VoxelPYTHON_wrap.cxx] Error 1
make[1]: *** [Voxel/SWIG/CMakeFiles/_Voxel.dir/all] Error 2
make[1]: *** Waiting for unfinished jobs....