This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLP4500与灰点相机问题



在按照TI提供的dlpu019a.pdf 进行学习时,我使用的是灰点相机 具体型号为CMLN-13S2M-CS

看了接口手册后  确定连线应该没错 大概示意图如下

启动应用后,出现以下错误

Connecting to projector...
Configuring projector...
Connecting to camera...
Configuring camera...
Camera setup FAILED!
ERRORS: 2 and WARNINGS: 0
ERROR: PG_FLYCAP_C_SET_FORMAT_7_FAILED
ERROR: CAMERA_NOT_SETUP


Please resolve the camera connection issue before proceeding to next step...


Texas Instruments DLP Commandline 3D Scanner

0: Exit
1: Generate camera calibration board and enter feature measurements
2: Prepare DLP LightCrafter 4500 (once per projector)
3: Prepare system for calibration and scanning
4: Calibrate camera
5: Calibrate system
6: Perform scan (vertical patterns only)
7: Perform scan (horizontal patterns only)
8: Perform scan (vertical and horizontal patterns)
9: Reconnect camera and projector

Select menu item:

请问会是什么原因 换了几根触发线还是不行?