现在用BBB的I2C接口控制DLPDLCR2000EVM输出自己用matlab生成的几幅图像,现在能用i2c控制输出几张内部测试图像,但现在想显示自己生成的条纹图像,可以只用i2c显示吗?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
现在用BBB的I2C接口控制DLPDLCR2000EVM输出自己用matlab生成的几幅图像,现在能用i2c控制输出几张内部测试图像,但现在想显示自己生成的条纹图像,可以只用i2c显示吗?
现在我就是用I2C控制,切换测试画面或Splash画面,但我想用自己的图像,所以如果用自己的图像替换内部测试画面或Splash画面呢?手册2.4.1.3-2说明,可以通过I2C更新里面的图像,但如果把图像通过I2C写入flash中呢,用什么工具吗?或如何把图像转成数据,谢谢
您好!
更新固件都需要通过I2C,主要的方式有
1.通过EVM的GUI软件,请参考

2.在编程手册的附件3中有Flash的地址映射,您可以参考2.3章节Flash Interface的介绍来手动修改里面的图片。但是目前没有直接的example给到您,推荐您先将flash image备份,再尝试修改图片。