This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLPC6401开机初始化屏幕旋转问题

Other Parts Discussed in Thread: DLPC6401

目前在使用DLPC6401做.45 1080P的DLP投影仪,主平台使用RK3128,目前遇到一个使用问题如下:请帮忙看下有无办法解决。

开机初始化配置屏幕旋转没有效果,开始初始化配置亮度没有效果。具体配置如下:

1、开机直接配置0X08和0X09寄存器,屏幕旋转没有效果,必须先配置0X00为1并延迟200ms后将0X00配置为0并延迟300ms后,在配置0X08和0X09才会有效果。但这样配置寄存器会出现一个结果,就是开机旋转画面会遇到:Logo画面,到测试画面,再到Logo画面,这样影响用户体验效果,请问有没有办法实现开机初始化旋转一直为Logo画面?

2、开机初始化配置亮度0Xcb寄存器没有效果,需要在开机30s(安卓系统启动之后),在配置0Xcb寄存器才会有效果,能否实现开机配置寄存器实现亮度的配置?