This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

1、DLPC350+dmd4500 去掉video模式之后,30bit信号,FPD信号也就是PORT1和port2部分的信号都没有输入,不需要接,那么这部分引脚是直接悬空吗?2、还有EVW中使用的FLASH目前已经停产了(不管是BOM中M29W128GL70N6F的还是原理图中的M29DW128GL70N),有没有推荐的FLASH可以使用?3、在使用中GPIO目前也没有用,请问是直接悬空还是需要上拉或者下拉?还有几个RESERVED pin是input 或者 biderection pin 是否需要上下拉?

Other Parts Discussed in Thread: DLPC350

1、使用中,我们去掉了video mode 只是用pattern sequence mode,所以PORT1和PORT2部分没有信号输入,请问这部分是直接悬空,还是需要有其他的外接电路?如果有,请问能给一个参考电路吗?

2、不管是BOM中M29W128GL70N6F的还是原理图中的M29DW128GL70N都已经停产了,请问有推荐的FLASH 可以使用吗?

3、现在的电路中GPIO也取消了,没有使用,请问是直接悬空还是需要接上拉或者下拉?

4、有几个RESERVED pin是input 或者 biderection pin,在dlpc350的datasheet中,第十一章中提到,如果没有使用的引脚是input或者biderection pin时,需要内部有上下拉电阻,如果没有需要外接。这几个引脚分别是:J2/F4

5、iic1和uart也是不适用的,请问是否直接悬空?

  • 您好!

    感谢您使用TI的DLP产品。

    1、使用中,我们去掉了video mode 只是用pattern sequence mode,所以PORT1和PORT2部分没有信号输入,请问这部分是直接悬空,还是需要有其他的外接电路?如果有,请问能给一个参考电路吗?

    可以直接悬空,PORT1/2的信号有内部下拉

    2、不管是BOM中M29W128GL70N6F的还是原理图中的M29DW128GL70N都已经停产了,请问有推荐的FLASH 可以使用吗?

    这个FLASH只需要满足DLPC350数据手册中关于flash的规格要求即可,可以参考如下帖子:

    3、现在的电路中GPIO也取消了,没有使用,请问是直接悬空还是需要接上拉或者下拉?

    External pullup or pulldown resistors may be required to ensure stable operation before software is able to configure these ports.最好可以接外部上拉或者下拉

    4、有几个RESERVED pin是input 或者 biderection pin,在dlpc350的datasheet中,第十一章中提到,如果没有使用的引脚是input或者biderection pin时,需要内部有上下拉电阻,如果没有需要外接。这几个引脚分别是:J2/F4

    J2和F4可以悬空,在TI的EVM上这两个Pin也是悬空的

    5、iic1和uart也是不适用的,请问是否直接悬空?

    可以直接悬空