This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLP LightCrafter 4500 无法正常连接pc问题

Other Parts Discussed in Thread: DLP4500

之前已有一套dlp4500,且能够在pc上正常操作;由于工作需要,我最近又新买了一套dlp4500投影模块,对新dlp4500接通12v电源之后,该投影仪按一定时间频率自动投影紫色图片,大概1s左右投影一张(应该是模块内置测试图片,闪的比较快,具体什么图看不清);在连接usb和hdmi之后依然按原固定频率投影紫色图片,且电脑中原来安装的gui界面显示没有连接(事实上原来那台dlp能够正常运行);不知道我中间是否漏了什么操作步骤,感觉软件控制端好像没打开似的,不知道您这边能否解答。

  • 您好!
    感谢使用TI的DLP产品。
    1.请检查连接线正常,包括与光机的flex cable以及LED的连接线是否接触正常。
    2.尝试连接J18,看是否可以连接到GUI,如果可以那么就重新更新下firmware。
    请先做如上测试,谢谢!