This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLP4500EVM能否自动从FLASH加载图片?

Other Parts Discussed in Thread: DLPR350, DLP4500

我司现在要设计一种三维测量产品。

下面想请教几个问题:

1. DLPC017B文档中,

Download the latest DLPR350 firmware version from the tool page. Extract the executable file from the
downloaded DLPLCR4500GUI-***-********.zip file and run it.

我进入网页下载的文件中,没有DLPLCR4500GUI-***-********.zip文件,能不能给出一个下载地址?

2. 一直没有找到这个文件DLPR350PROM_v2.0.0.bin,能不能提供一下? 

3. DLP4500EVM是否支持自动循环从FLASH加载图片到BUFFER中?

盼回复!

  • 您好!

    感谢使用TI的DLP产品。

    1.

    2.

    3.可以通过配置sequence实现。

    谢谢

  • 3. DLP4500EVM是否支持自动循环从FLASH加载图片到BUFFER中?
    这个问题,我反复看了你提供的PDF用户手册,还是搞懂350是如何“自动循环”从FLASH加载图片的?
    手册只说了,图片加载到BUFFER后,怎样自动循环PLAY。没有提到循环加载图片?
    我是想知道 如何“自动循环”从FLASH加载图片的?
    请指点下。
  • 您好,通过UM232H JTAG Flash Programmer,Erase Flash 正常,Program Flash 到20%,突然就到100% Complete,但去掉J30,上电,DLP4500还是不能点亮,这然还能怎么处理吗

  • 可以通过GUI配置pattern sequence来实现。
    1、先通过GUI将多张图片合并成每张24bit的912*1140分辨率的图形;
    2、将该图片添加到TI原始固件firmware1,生成新的固件firmware2;
    3、将firmware2通过GUI烧录到DLP,并根据需要配置pattern sequence,包括工作模式,亮度,配置图片顺序,触发模式、曝光时间,曝光周期等,并点击save solution,保存配置的ini文件;
    4、将该ini文件与firmware2通过GUI合并生成新的固件文件firmware3;
    5、将该固件firmware3通过GUI烧录到DLP中,如果步骤3中配置的是internal trigger,上电时就会根据配置自动投影配置的图片序列。如果配置的是external trigger,则会等待外部trigger信号通过J11输入同步信号后,根据同步信号来投影。