This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

请教DLPC3438的一个黑白屏故障问题



使用3438+3000的方案,.3的光机,投影仪在使用一段时间之后出现屏幕变成黑白屏,原彩色画面变为黑白色且画面锁住不动。

排查外围电路,信号和各路电源以及三路偏置电压都是正常的,iic读3438的寄存器状态跟正常时候的比较也是一致。

INT信号通过手动拉低,可以重新刷新画面,即一个视频其实是在正常播放,手动刷新可以将黑白画面变为当前一帧,随即锁住不动。

目前没有头绪该如何入手,没有报错信息,除了project on重新打开外没有其他方法恢复。

请大家指教,给点思路,谢谢