This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
EVM软件版本是6.1.2,EVM firmware版本是0.0.5,gui software版本是1.1.0.7
我的操作流程是这样的:在菜单项light control 的 internal patterns页 设置好了pattern sets,设置好了pattern order,然后点击program pattern data按钮下载图片。
这一切都操作完成后,如果我不勾选trigger in 的enable,直接点击run once,是可以正常投影的。但是如果我勾选了trigger in 的enable,Polarity是active high,这时我再点击run once ,然后给板子一个3.3v的信号,是不会有投影的。正极接的板子j4的第5口,负极接的j4的第1口, 给的input信号是3.3v没错,用示波器量过了。搞了一下午,不知道该如何继续查找问题所在了。
您好!
感谢使用TI的DLP产品。
原理图中J4的Pin7是Trig_OUT_1,Pin4是Trig_OUT_2,Pin1是地。
请参考DLPC3478 Datasheet 信号定义,TSTPT_4是Trig_OUT_1,GPIO_7是Trig_OUT_2.
谢谢!