This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLP4500EVM的LED问题导致DLPC350重启



你好

我按照官方4500EVM的原理图自己做了开发板。在使用中遇到了在GUI中调大LED电流导致DLPC重启的问题

默认使用时,调整LED电流为104,可以正常工作,但是当加大电流到200以上时,LED亮一下后立刻重启。

我们使用同一个电路板更换了光机,可以将这个值调到255,问题不会出现。我们使用同样的光机更换电路板,问题依旧存在,因此将问题锁定在LED上。

如果手动拉低EN,然后先调节电流到200以上,再拉高EN,同样是LED闪一下后DLPC马上重启。

我们的LED驱动部分原理图如下:和官方原理图一致

温度检测的功能没有使用。这个驱动只接收LED_EN与LED_PWM信号。调节电流值会影响PWM的低电平占空比。在LED_EN没有拉高的时候,调节PWM值都可以正常设置。一旦EN拉高,出问题的光机会立刻导致DLPC重启。然而在电路板正常工作的情况下,拔下LED灯使驱动断路,或者短接LED的正负极使驱动短路都不会导致DLPC重启。而且EN与PWM都是DLPC的输出信号,驱动也没有其他信号反馈给DLPC。

那么

1,为什么LED驱动的问题会导致DLPC重启?

2,LED短路或者断路都不会导致DLPC重启,那LED在什么状态会导致DLPC重启?