使用的是3010evm,但是开机之后不投开机画面,指示灯都正常亮,但是控制GUI上,显示Connected,Powered Off。
不知是什么问题,有解决的方法吗?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
使用的是3010evm,但是开机之后不投开机画面,指示灯都正常亮,但是控制GUI上,显示Connected,Powered Off。
不知是什么问题,有解决的方法吗?
您好!
感谢使用TI的DLP产品。
请问使用的是哪款EVM?是DLP3010 LC EVM吗?
该EVM的状态说明如下:
Ready – the EVM has power, is connected to your PC using USB, and isturned on.
Connected, Incompatible EVM – the EVM connected is not meant to be used withthe current EVM tool or is not recognized. Some commands may not work as intended.
Connected, Powered off – the EVM has power and is connected to your PCusing USB, but is not turned on. The EVM must be turned on to use most featuresof the PC software.
Not connected – the EVM is not connected using USB, or is not connectedto a power source.
如果是Connected, Powered off代表着系统没有上电。请检查SW1是否处于on状态。
板上LED状态是什么样子的?(D1、D2、D3、D5和D6)
谢谢