This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLP LightCrafter6500 EVM添加图片的疑问



DLP LC6500EVM 的User"s Guide 中,3.9.1 Adding or Removing Patterns from the Firmware提到:

“the GUI will pack the images into groups of 24-bit RGB bitmap images. This means if there are 1-bit black and white images, 8-bit gray scale images, or anyother image bit-depth (up to 24-bit images), they will be combined to create a composite image. Forexample, a composite image could be composed of 24 1-bit images, 3 8-bit images, or a combination of images of various bit-depths which add up to a 24-bit composite image”

也就是说输入24幅1位图片GUI会组合成一张24位的图片?请问这是怎么做到的,那24张的一位图片和24位的图片是什么对应关系呢?比如我有一张24位的图片,能不能把它分解成24张1位图片?

感谢解答

  • 您好!

    感谢使用TI的DLP产品。

    一张24bit图片与24张1bit图片的关系如下图所示:

    谢谢

  • 您好,感谢您的解答。24位RGB图像分成R、G、B的单通道图像很好理解,但是像上图,8位图像怎么分成8张1位图像的呢?位平面分解?感觉不是很像啊,位平面分解后后面几张图像都是马赛克一样,还能合成原来的图像吗?对这个确实没有理解清楚,求解答,谢谢~非常感谢
  • 您好!
    图片只是一个示例,可以忽略颜色和每个位平面的内容,实际就是按位平面分解。
    在实际上的使用中,通常是根据需要使用的pattern来合成24bit的图片,然后在pattern sequence中配置相应的pattern并显示。DLP4500EVM支持1-8Bit的pattern显示。
    谢谢