请问有谁用过TI的DLP3310这款光机么?请教以下几个问题:
1.可以外部触发两个相机采集图像吗?;
2.针对1920*1080分辨率的24位图片,其投射的频率是多少?最快可以达到多少呢?
3.该光机跟DLP4710的区别在哪?在做结构光扫描方案时,哪个更有优势?
若有了解的,请解答一下,非常感谢啦!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
请问有谁用过TI的DLP3310这款光机么?请教以下几个问题:
1.可以外部触发两个相机采集图像吗?;
2.针对1920*1080分辨率的24位图片,其投射的频率是多少?最快可以达到多少呢?
3.该光机跟DLP4710的区别在哪?在做结构光扫描方案时,哪个更有优势?
若有了解的,请解答一下,非常感谢啦!
您好!
感谢关注TI的DLP产品。
1.可以外部触发两个相机采集图像吗?
DLPDLCR3310EVM主要用于显示应用,比如微投、无屏电视等,基于DLP3310+DLPC3437芯片组,并没有针对3D扫描应用的触发信号与相机同步。
2.针对1920*1080分辨率的24位图片,其投射的频率是多少?最快可以达到多少呢?
在显示应用中,支持1080P@60Hz
3.该光机跟DLP4710的区别在哪?在做结构光扫描方案时,哪个更有优势?
DLP3310和DLP4710的面板大小不同,如果是应用在结构光扫描应用时,建议使用DLP4710,DLP4710可以与DLPC3439搭配使用应用在显示应用中,同时DLP4710也可以与DLPC3479搭配使用,应用在结构光等工业应用中。
DLPC3479增加了同步触发输入和输出信号,以及1bit/8bit pattern 投射功能,请参考:
http://www.ti.com.cn/tool/cn/DLP4710EVM-LC?keyMatch=DLP4710&tisearch=Search-CN-Everything
另外也可以考滤DLP3010EVM-LC, LightCrafter4500EVM等,专门针对结构光扫描应用:
http://www.ti.com.cn/tool/cn/DLP3010EVM-LC?keyMatch=DLP3010&tisearch=Search-CN-Everything
http://www.ti.com.cn/tool/cn/DLPLCR4500EVM?keyMatch=DLP4500&tisearch=Search-CN-Everything
谢谢
您好!
区别在于DLP4710的控制器不一样,DLP4710EVM-LC使用DLPC3479,且具有触发输入输出,DLPDLCR4710EVM-G2使用DLPC3439应用于显示应用。建议使用DLP4710EVM-LC。
谢谢