DLP4500设置好内触发模式开始投影并向相机发送触发信号,同时用VS打开相机设置为外触发模式,这样可以直接触发拍照吗,还是需要调用DLP的API检测触发信号来控制拍照
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
DLP4500设置好内触发模式开始投影并向相机发送触发信号,同时用VS打开相机设置为外触发模式,这样可以直接触发拍照吗,还是需要调用DLP的API检测触发信号来控制拍照
您好!
可以将相机配置为外部触发模式,然后使用DLP4500输出的触发信号来触发相机拍照,也可以使用相机的输出来触发DLP4500投影。可以直接使用相机的SDK来配置相机工作模式。
如果是想使用TI的3D scan demo的SDK,那么在C:\TexasInstruments-DLP\DLP-ALC-LIGHTCRAFTER-SDK-2.0\DLP-ALC-LIGHTCRAFTER-SDK\src\camera\pg_flycap2\pg_flycap2_c.cpp中具有对相机的配置函数。

谢谢