This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TI DLP9500 DLPC410咨询

Other Parts Discussed in Thread: DLPC410

  1. 购买TI开发板能否拿到代码或IP方面的资料?

  2. 目前TI官网上的DLPC410是基于VIRTEX 5来实现,麻烦帮忙确认我们设计时是否购买DLPC410就是找TI购买一颗VITEX 5的芯片,再加一颗DLPR410的配置文件

  3. 我们能否将DLPC410的配置加载到其它FPGA芯片里,我们在设计时,可以只用一颗FPGA来实现图像处理和DLP驱动控制

  • 您好!

    感谢使用TI的DLP产品。

    购买TI开发板能否拿到代码或IP方面的资料?

    ->Discovery4100开发板上有两颗FPGA,Applications FPGA的代码是开放的,可以在ti.com上下载得到:

    但是并不提供DLPC410的源码。

    目前TI官网上的DLPC410是基于VIRTEX 5来实现,麻烦帮忙确认我们设计时是否购买DLPC410就是找TI购买一颗VITEX 5的芯片,再加一颗DLPR410的配置文件

    ->是的,需要向TI采购DLPC410和DLPR410

    我们能否将DLPC410的配置加载到其它FPGA芯片里,我们在设计时,可以只用一颗FPGA来实现图像处理和DLP驱动控制

    ->不能使用其他FPGA,DLPC410的目的除了实现对DLP的控制,也是为了防止保护DLP芯片不受错误控制造成的损害。

    谢谢