您好,在利用DLP4500成功烧录入一组图案后,怎样通过软件(或投影仪的api)实现控制DLP4500投影仪投影指定的图案。
例如,我烧录5张图案至DLP4500,现在我想在自己开发的软件上实现控制投影仪投影其中任意一幅图案,后续应该如何操作?
谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好!
这个功能是可以实现的,但是首先想确认如下问题:
1.是希望实现pattern功能,还是显示flash中的图片?
2.5幅图像是几位的?
3.目前是使用什么方式依次投射1-5幅图案的?是使用GUI还是软件?可以提供具体的配置吗?
谢谢
您好!
谢谢分享。如果您是使用的GUI源码中的int DLPC350_PatternDisplay(unsigned int Action)函数,那么该函数实际只是发送了一个Start命令,对应DLPC350寄存器为0x65。
但是在start前需要先配置sequence,在DLPC350 programmer guide中有配置pattern sequence的example(4.1节),可以参考example来配置pattern投射。其中0x78寄存器可以配置想要使用图像的index,pattern的位宽等参数,实现灵活配置。
谢谢
您好!
请参考Lightcrafter4500EVM USer Guide 3.5节

Best regards