我们希望开发自己的光谱分析仪,使用TI 的DLPC150和DMD 2010NIR,但是看了相关文档后,并未看到说明信息,是通过MCU和DLPC间的RGB总线传输图像,从而控制微镜的翻转吗?
而且DLPC150和DMD 2010NIR间的通信协议是什么?传输的DATA和CLK如何控制每一个微镜单元的翻转呢?能不能提供一些资料呢?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我们希望开发自己的光谱分析仪,使用TI 的DLPC150和DMD 2010NIR,但是看了相关文档后,并未看到说明信息,是通过MCU和DLPC间的RGB总线传输图像,从而控制微镜的翻转吗?
而且DLPC150和DMD 2010NIR间的通信协议是什么?传输的DATA和CLK如何控制每一个微镜单元的翻转呢?能不能提供一些资料呢?
您好!
感谢关注TI的DLP产品。
是通过MCU和DLPC之间的RGB总线来传输图像并控制微镜的翻转的。DLPC150和DLP2010NIR之间的通信协议并不开放,目的在于降低客户开发难度以及保护DLP芯片。DLPC150会自动实现将RGB输入的信号转换为DLP能够识别的信号并发送给DLP芯片。可以通过控制输入的RGB信号来控制相应的微镜。
参考设计:
http://www.ti.com.cn/tool/cn/TIDA-00554#technicaldocuments
EVM:
http://www.ti.com.cn/tool/cn/DLPNIRNANOEVM
谢谢
您好!
您的理解没有问题,这只是一个bit-plane。但是这些操作会有DLPC150完成,不需要用户控制。
谢谢