1.我理解图片像素和DMD的微镜阵列之间是1对1映射的,那我应该怎么样制作对应的二进制图像,图片像素有什么格式推荐吗
2.在查看dlpa008b里面了解到DMD有微镜定时脉冲模式,我想咨询下能否介绍在控制芯片比如DLPC3470中如何用指令实现block mode,快速置位和复位数据
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
1.我理解图片像素和DMD的微镜阵列之间是1对1映射的,那我应该怎么样制作对应的二进制图像,图片像素有什么格式推荐吗
2.在查看dlpa008b里面了解到DMD有微镜定时脉冲模式,我想咨询下能否介绍在控制芯片比如DLPC3470中如何用指令实现block mode,快速置位和复位数据
您好!
感谢使用TI的DLP产品。
DLPC3470可以与DLP2010或者DLP2010NIR搭配使用,分辨率为854x480.
如果需要实现标题中DMD按照时间顺序逐次打开一定行数的微镜阵列,同时其他阵列处于关闭状态的功能,可以通过依次输入只有一定行数为1,其余为0的1bit 图片(pattern),则可以控制相应的微镜打开,而其余的处于关闭状态。图片需要预先保存自Flash中或者从外部视频接口输入,对图片格式无要求.
DLPC3470不能单独控制某个block,定时脉冲也会自动发送,不需要单独控制。DLPC3470最高支持2500Hz(1 位)和 360Hz(8 位)的pattern速度。
请参考DLPC3470数据手册:
谢谢