你好,我使用的是DLP4500,现在我想在QT中自己编写一个简单的程序来控制投影仪中的一部分简单功能,我已经按照dlpu042--开发套件电脑配置中,配置好了,我在dlp4500的gui文件中找到了源代码,但是现在我不知道这些文件具体是什么功能,是否有说明书或着是相关的介绍之类,我在论坛里找了很久都没找到,希望您能详细回答,辛苦您了!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好!
感谢使用TI的DLP产品。
LightCrafter4500 EVM的GUI源码的API是一系列的I2C/USB命令,很遗憾目前并没有专门的说明文档来介绍其具体功能,但是在源码中提供了较为丰富的函数说明,可以帮助理解每一个 函数的具体功能。
建议结合DLPC350 Programmer guide来理解:
http://www.ti.com/lit/ug/dlpu010g/dlpu010g.pdf
谢谢