在以下文档里 《Introduction to ±12 Degree Orthogonal Digital Micromirror
Devices (DMDs) 》提到Phased Mirror Clocking Pulse Steps 的工作模式,见(文档中的4.3.2章节,figure4-7);
请问DLPC150搭配DLP2010NIR 能支持这种模式吗?
如果支持的话,这个pulse信号能否由MCU读到呢?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
在以下文档里 《Introduction to ±12 Degree Orthogonal Digital Micromirror
Devices (DMDs) 》提到Phased Mirror Clocking Pulse Steps 的工作模式,见(文档中的4.3.2章节,figure4-7);
请问DLPC150搭配DLP2010NIR 能支持这种模式吗?
如果支持的话,这个pulse信号能否由MCU读到呢?
您好!
在DLPC150+DLP2010NIR的系统中,用户不能单独发送 Phased Mirror Clocking Pulse,所有DLP的mirror的控制全部由DLPC150完成。
在上述24-bit Parallel Port Streaming Pattern 中,客户只需要配置DLPC150到相应的模式,然后输入需要的pattern data,DLPC150就会自动完成所有DLP控制操作。
谢谢
您好!
很抱歉造成您的误解。
我指的模式是指DLPC150的工作模式,比如24-bit Parallel Port Streaming Pattern模式、16-bit Parallel Port Streaming Pattern模式,Flash Pattern Display模式等,无法配置phase move运行模式。
Phase move模式主要是在一些尺寸更加大的DLP中可以控制,用户有更高的控制权限:比如DLPC410、DLPC910等。
针对您的应用,可以这样理解在trigger out的脉冲内,mirror是处于stable的状态。如果需要实现按行或者按列扫描,那么只需要输入行或列的bitplane(pattern)即可。
谢谢