Other Parts Discussed in Thread: DLP3010EVM-LC, SN74AUP2G07
现用DLP3010evm-lc的trigger out2接工业相机的光耦输入,但是无法触发相机拍照,用信号发生器设置同样的波形就可以触发相机拍照。
是否是trigger out的驱动能力不足?该如何解决?
工业相机输入原理如下:
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: DLP3010EVM-LC, SN74AUP2G07
现用DLP3010evm-lc的trigger out2接工业相机的光耦输入,但是无法触发相机拍照,用信号发生器设置同样的波形就可以触发相机拍照。
是否是trigger out的驱动能力不足?该如何解决?
工业相机输入原理如下:
您好!
DLP3010EVM-LC上使用的是SN74AUP2G07:http://www.ti.com/cn/lit/ds/symlink/sn74aup2g07.pdf
其负载电流需小于20mA:
而且截图中的输出电压基本是可以到3.3V,如果驱动能力不够应该到不了3.3V。但是不清楚为什么无法驱动您的相机。
3010EVM-LC R35改动trigger in上拉电平后使用正常。
是需要使用Trigger in吗?为什么需要修改R35上拉电平?3DR信号是1.8V的
上电EVM发热冒烟导致散热片塑料处融化。目前PC无法识别EVM。
安装或者焊接过程中可能造成短路或者其他的损坏,建议您检查硬件电路,比如电源轨等,尤其是冒烟发热的部位。
Best regards