This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

RGB666接口的处理器如和接DLPC3435上?

Other Parts Discussed in Thread: DLPC3435

RGB666接口的处理器如何接到DLPC3435上?是将DLPC3435的RGB888低两位都悬空?还是将低两位接到接到R7 G7 B7上??

  • 您好!

    感谢使用TI的DLP产品。

    请参考DLPC3435的数据手册,I/O Mapping。

     

    http://www.ti.com/cn/lit/ds/symlink/dlpc3435.pdf

    Best regards

  • 您好!感谢回复!
    数据手册有看过,所以才会有疑问,一般RGB888接口的低两位悬空就是RGB666,
    数据手册中插图描述不理解,ASIC input Mapping是指其他RGB666接口的处理器?
    ASIC internal Re-Mapping是指DLPC3435吗?RGB低两位不是悬空就可以了吗?
    一定要将RGB低两位接在R7 G7 B7上吗?急~盼回复!
  • 您好!

    ASIC Input Mapping是DLPC3435上的Parallel 接口,如下图:

    在RGB666输入的情况下使用的是PDATA_17-PDATA_0

    ASIC Internal ReMapping是DLPC3435内部完成的,DLPC3435会将RGB Channel最高位的bit填充到最低位来组成24bit数据,这是DLPC3435内部完成的不需要控制。

    您需要做的是将PDATA_17-PDATA_0(18bit)连接到前端处理器上。不知道这样解释是否清楚

    Best regards

  • 您好!
    感谢回复,解释的很清楚,已经明白了。再次感谢!
  • 您好!
    还有几个问题点需要确认!
    (1)RGB666从低到高位是对应DLPC3435从PDATA_0到PDATA_17对吧?(即B0-B5对应PDATA_0---PDATA_5,G0-G5对应PDATA_6---PDATA_11,R0-R5对应PDATA_12---PDATA_17)
    (2) 如果我们前端处理器输出RGB888并将低2位接地,这样做成RGB666,对应到DLPC3435的RGB888。这样做和规格书中要求的将PDATA_17-PDATA_0(18bit)连接到前端处理器有什么差异或者我们以RGB888做RGB666的做法有什么风险?
    (3)目前以规格书中要求的将PDATA_17-PDATA_0(18bit)连接到前端处理器调试,发现图像扭曲。我们前端处理器输出的是RGB888去掉了低2位,接到DLPC3435是规格书中要求。图像扭曲问题出在哪里?
  • 您好!

    (1)(2)应该是没有问题的

    (3)请问是否有配置外部视频源的格式?默认是RGB888,如果没有请参考DLPC3435编程手册:

    http://www.ti.com/lit/ug/dlpu020c/dlpu020c.pdf

    请问您是应用在什么样的应用中?为什么不使用RGB888?

    Best regards

x 出现错误。请重试或与管理员联系。