为更好的满足我们的研发需求,我们需要对DDC4100这个软件进行二次开发,使用的方法是基于Active控件,参考的设计文档是dlpu039,在设计过程中出现了一个问题,希望可以帮助解决疑惑
问题:是否存在一个初始化过程,我在按照文档进行图片导入的时候发现自己研发的软件无法成功导入图片,但是在使用官方提供的DDC4100软件成功导入一张图片后,再使用自己研发的软件就可以成功导入图片了,所以我是不是少了一些初始化的函数?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
为更好的满足我们的研发需求,我们需要对DDC4100这个软件进行二次开发,使用的方法是基于Active控件,参考的设计文档是dlpu039,在设计过程中出现了一个问题,希望可以帮助解决疑惑
问题:是否存在一个初始化过程,我在按照文档进行图片导入的时候发现自己研发的软件无法成功导入图片,但是在使用官方提供的DDC4100软件成功导入一张图片后,再使用自己研发的软件就可以成功导入图片了,所以我是不是少了一些初始化的函数?
您好!
文档中确实没有该函数的说明,但是从描述看该函数的功能是write image to DMD和发送MCP,请尝试使用如下两个函数代替该功能。
Short LoadToDMD (short BlockNum, short DoReset) ;
Short Reset(short BlockNum) ;
DLPC410的工作方式请参考:http://www.ti.com/lit/ds/dlps024f/dlps024f.pdf
Best regards