This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我们现在做了一块dlpc3478+dlpa3000的线路板,连接DLP3010 EVM-LC的光机。但是无法启动,host_irq脚无法拉低。
示波器观察spi1上电后无信号,请帮忙分析是什么问题。
firmware是之前ti工程师给的,Option1。上电后,spi0 有一段信号。
所以想问下,option是否正确,或是其他问题,谢谢!
您好!
感谢使用TI的DLP产品。
DLP3010EVM-LC上是option 1,请参考EVM的User Guide。
http://www.ti.com/lit/ug/dlpu070b/dlpu070b.pdf
Option选项并不会影响系统的正常启动。
Best regards
我手里有一块DLP3010 EVM板,但底板比较大,我想自己做一块底板,缩小产品的尺寸,做结构光控制用,请问底板上的MSP430有什么作用?我用I2C控制控制DLP在自己做的底板上可以删除MSP430和HMDI这里东西吗
您好!
MSP430主要负责上下电控制以及配置周边芯片,比如ITE6801(HDMI),如果有其他替代的方案是可以删除的。
Best regards