DLP9500
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好!
感谢关注TI的DLP产品。
1.DLPC410芯片手册、DLPA200芯片手册、DLP9500芯片手册都没有关于控制寄存器的描述,软件如何开发?如果是TI提供固件代码,请问在什么地方下?如何配置这些固件为我想要的工作方式?是不是买DLPC410时软件已经烧好了?
->DLPC410、DLPA200和DLP9500中,DLPC410是需要固件的,其固件已经烧录在DLPR410中,其软件不需要任何修改。您需要做的是开发K7中的代码。
2.K7里面代码开发需要参考那些资料?TI提供了APP FPGA源码VHDL,我应该如何利用这些源码,改变成可以在K7中运行的Verilog代码?
->APPs FPGA的VHDL源码是为了EVM的使用开发的参考代码,您可以按照DLPC410的数据手册(同时参考VHDL)开发verilog程序,没有特定的要求。硬件部分可以参考TI的参考设计:
https://www.ti.com/tool/DLPLCRC410EVM
https://www.ti.com/tool/DLPLCR95EVM
3.我们想脱离PC机,直接实现一个相机和DMD的通信,请问是否支持,如果支持,我们应该怎么做?
->请问具体的引用场景是怎么样的?可以脱离PC,需要自行开发Apps FPGA中的代码
Best regards
您好!
请参考另一个帖子中的回复。

Best regards