This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
我i这边设计了一块DLPC3478的电路板,参考demo线路设计,其中HOST_IRQ信号上电后一直为高,没有拉低,按照3478手册上的时序要求,只有当HOST_IRQ信号变低之后,I2C通信才被允许,请问这个HOST_IRQ信号一直为高的原因是什么呢?
另外,CY7C65215这颗USB转I2C的芯片裸板是否需要烧录固件,烧录方式是怎样的,麻烦提供下,谢谢
您好!
正常启动要求:DLPC3478必须要烧写固件,同时连接LED和DMD。
固件下载:http://software-dl.ti.com/dlp/pico-fw-selector/
烧写方式:
1.使用Flash烧录器裸片烧写,然后再焊接到板子上
2.使用GUI,要求板上有CYPRESS芯片,同时SPI口连接到FLASH(与EVM相同)
3.有前端处理器,并且链接SPI到FLASH,也可以直接使用处理器烧写
关于CY7C65215,这并不是TI的芯片,其配置软件请从Cypress官网下载。
Best regards
您好!
由于CY7C65215不是TI的产品,我没有办法提供其调试软件,请与CYPRESS联系。
GUI在DLP系统启动之前是不会显示连接成功的,但是不应该影响SPI的烧写,请尝试:
烧写MSP430的代码,下载链接:https://www.ti.com/tool/DLP3010EVM-LC
确保Proj_on处于OFF,FLASH和CY7C65215处于上电状态。
或者直接离线烧写Flash。
Best regards,
Kevin
您好!
如果430还是没有烧写代码,请上拉Cypress芯片的GPIO6,再测试
GUI本身会自动配置Cypress芯片的,如果需要也可以尝试从TI的EVM中导出其配置文件,再烧写到板子上。
Best regards