This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLP2010evm-lc 混合internal pattern set显示问题

比如当我添加一个包含8个1D的vertical pattern和一个包含8个1D的horizontal pattern,这种混合的pattern set显示有问题,只会播放第一个pattern set里面的8个pattern,之后就一直黑屏了。这个问题怎么解决?

EVM software version: 8.1.0

EVM firmware version: 8.0.0

GUI software version: 2.2.0.6

  • 由于国庆假期,我们建议您将问题发布在E2E英文技术论坛上http://e2e.ti.com/support/dlp/f/94,将由资深的工程师为您提供帮助。我们的E2E英文社区有TI专家进行回复,并得到全球各地工程师的支持,分享他们的知识和经验。

  • 您好!

    感谢使用TI的DLP产品。

    请问具体是如何配置的?除了在pattern set中加入pattern以外,同样需要在pattern set display order中加入显示顺序。

    Best regards

x 出现错误。请重试或与管理员联系。