我想事先烧录一组图案至dlp6500的固件内,然后利用上位机软件调用dlpc900 SDK提供的API来控制投影仪,通过指定图像索引来投影我想要投影的某一张图案。这个功能我之前在利用dlp4500的投影仪完成过,当时利用的是dlpc350的SDK内部的API,但是现在我想在dlp6500的固件上实现同样的功能。本来我想仿照之前调用dlpc350 SDK的API来调用类似的dlpc900 SDK的API以实现该功能,但我发现dlpc900 SDK内部与之相关的一些API只有函数声明,但其内部代码并没有实现,并且有些函数头注释是沿用dlpc350的函数注释,如下图所示:
dlpc900 SDK类似的问题还有很多,请问我该如何利用该SDK实现dlp6500投影指定图案?