This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

The CC3200 MQTT_Client routine cannot connect to the server, as detailed below

Other Parts Discussed in Thread: CC3200

 [2020-10-31 16:01:16.850 R]



         *************************************************

            CC3200 MQTT_Client Application       

         *************************************************





[2020-10-31 16:01:17.510 R]

Host Driver Version: 1.0.1.11

Build Version 2.0.7.0.31.0.0.4.1.1.5.3.3


[2020-10-31 16:01:17.815 R]

Device is configured in default state 


[2020-10-31 16:01:17.920 R]

Started SimpleLink Device: STA Mode


[2020-10-31 16:01:18.636 R]

[WLAN EVENT] STA Connected to the AP: TP-LINK_511 , BSSID: b8:f8:83:f4:3d:f6


[2020-10-31 16:01:19.381 R]

[NETAPP EVENT] IP acquired by the device


[2020-10-31 16:01:19.970 R]

Device has connected to TP-LINK_511

Device IP Address is 192.168.1.160 



[2020-10-31 16:01:21.810 R]

Version: Client LIB 1.4.0, Common LIB 1.5.0.

C: Alloc for 1 2001dd34


[2020-10-31 16:01:22.466 R]

C:FH-B1 0x10 to net 16, Sent (161 Bytes) [@ 5]

C: Alloc for 0 2001dd34


[2020-10-31 16:01:22.551 R]

C: Rcvd msg Fix-Hdr (Byte1) 0x20 from net 16 [@ 5]

C: Msg w/ ID 0x0000, processing status: Good

C: RX closing Net 16 [4]

C: Cleaning session for net 16


Broker connect fail for conn no. 1 


[2020-10-31 16:01:23.546 R]

C: Net 16 now closed

disconnect from broker a1F8fKxfuZB.iot-as-mqtt.cn-shanghai.aliyuncs.com


 Exiting the Application