This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLP6500外部触发问题



你好,目前我使用DLP6500控制板从J24设置外部触发信号3.3V接到灰度相机触发相机采集,J25跳线已接,我现在在设置了如下两个模板,如图中所示,我连接的是trigger out1 触发,但是软件界面没有trigger out1设置,只有out2,而且好像不在软件界面设置也能触发,有点疑惑,这是第一个问题;第二个问题是我触发了后,比如我相机曝光设置10ms,第一个DMD模板设置5,第二个模板设置3,第三个模板设置2,触发后相机好像只是拍到了第一个和第二个模板的图案,好像加上dark time也没用,不知道问题出在哪