This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLP3478 是否可以设置上电就进入internal pattern mode进行投图

Other Parts Discussed in Thread: DLPC3478, DLP3010, DLP4500

您好!

     DLP3010+DLPC3478目前开机是一张splah图片,是否可以通过更改固件让开机就进入internal pattern mode 进行投图呢,同时trigger也默认配置。

    因为DLP4500通过更改ini文件是可以做到这样的,我想实现和4500一样的功能,请问是否可以实现?

谢谢!

  • 您好!

    感谢使用TI的DLP产品。

    DLPC3478同样可以实现该功能,可以使用GUI重新编译固件,在固件中加入配置好的pattern数据(.bin),同时加入batch file文件(类似于.ini),在batch file中加入模式控制以及触发信号的控制。

    Best regards