This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

基于DLPA3000+DLPC3470设计,20%左右板子显示有条纹问题

Other Parts Discussed in Thread: DLPC3470

您好,我们自己用DLPA3000+DLPC3470设计了产品,FPGA输出RGB888图像到DLPC3470,RGB888信号串联33R电阻。做板子50套,发现有10套板子工作20~60分钟后,出现竖条纹显示问题。用示波器探头测试 PCLK信号,点靠近FPGA端,图像显示正常;点靠近DLPC3470端,竖条纹问题更严重。

  • 您好!

    感谢使用TI的DLP产品。

    首先需要确认问题是否是由前端造成的,请问目前使用的是什么模式?如果切换到Splash或者Test pattern会不会出现这种情况?

    如果只在外部视频模式下出现那么需要检查如下方面:

    1.是否是视频信号本身的问题,检查Parallel Interface Frame Timing Requirements是否满足要求,请参考DLPC3470数据手册6.12节

    2.如果怀疑信号问题,那么请测试靠近DLPC3470输入端的信号是否满足规格要求。

    3.增加系统散热比如FPGA是否会有改善?

    Best regards