This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLP4710LC 与DLP4710区别?

Other Parts Discussed in Thread: DLP4710LC, DLP4710, DLPA3005, DLPC3439, DLPC3479, DLPA3000

请问DLP4710LC 与DLP4710有哪些区别?我要用DMD做光反射控制,只控制让DMD的相应的行列的微镜打开或关闭,并且在一段时间保持固定的状态不刷新,LED光源也不使用DLPA3005控制,这样的系统是要用DLP4710LC去实现吗?

  • 还请问下,如果给DLPC3439输入一个静态的纯黑白网格图片,DLP4710的微镜是一直保持静态不变,还是会一直刷新开关状态?怎样让DMD的微镜单元可以一直保持不变的状态?
  • 您好!

    感谢关注TI的DLP产品。

    DLP4710A与DLPC3439搭配使用,主要用于投影显示易用。

    DLP4710LC与DLPC3479搭配使用,主要用于工业应用比如3D扫描,3D打印。如果需要实现“只控制让DMD的相应的行列的微镜打开或关闭,并且在一段时间保持固定的状态不刷新”建议使用DLP4710LC。

    ”LED光源也不使用DLPA3005控制“,DLP系统相应的电源芯片比如DLPA3005或者DLPA3000等是为DLP系统供电的,如果没有该电源芯片会导致系统启动问题。

    Best regards

  • ,您好:

    请问DLP4710LC怎样用1bit数据模式,让DMD微镜保持静止的开关状态不刷新,等输入新的1bit数据后再刷新微镜的开关状态?

  • 用DLPA3005 芯片为DLP系统供电,但是不接LED,是否需要TI提供用特定的固件?
  • 您好!

    请问您需要使用在什么样的应用中?

    请问DLP4710LC怎样用1bit数据模式,让DMD微镜保持静止的开关状态不刷新,等输入新的1bit数据后再刷新微镜的开关状态?

    ->DLP4710LC+DLPC3479有pattern mode可以将需要显示的1bit数据保存在flash中,也可以从外部video接口输入,可以发送I2C命令控制pattern sequence的工作,也有Trigger in模式,具体请参考DLPC3479数据手册的pattern模式。

    DLPA3005 芯片为DLP系统供电,但是不接LED,是否需要TI提供用特定的固件?

    ->需要定制固件

    Best regards

  • 用来做空间光调制,需要让DMD的相应行列打开或关闭并保持状态不变。如果采用发送I2C命令控制pattern sequence的工作,不更新pattern sequence数据时,DMD的微镜单元可以保持状态不刷新吗?
  • DMD的微镜在投影1bit的pattern时是保持不变的,其投影时间由配置的曝光时间决定。
    Best regards