This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
实验环境:
1.DLP3010+DLPA3000+DLPC3478,可以正常投影工作
2.DLPA3000的78引脚接了热电偶100K上拉30K到DLPC3478GPIO_11(评估版接法)
问题:
1.Information首页 Temperature读数是谁的温度?
DLP3010芯片?
DLPA3000芯片?
DLPA3000的78引脚外挂的100K热电偶放置处的温度值?
DLPC3478芯片?
2.为什么Temperature读数是0,需要修改哪里能读出真实数值?
3.这个温度的获取方式是i2c访问Read System Temperature (D6h)地址读回值?