This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLPC350: DLPC350的I2C快速模式无法通信,标准模式不稳定

Part Number: DLPC350


现象:I2C快速模式400KHZ完全无法通信,DLPC350没有给任何的ACK信号,标准模式100KHZ能正常通信但是不稳定,会出现送出的SUBADDR没有ACK的问题,大部分时候都能正常通信,但是只要两次操作时间间隔小于200ms就经常出错,所以I2C的地址是没有问题的

如图是高速示波器抓的400KHZ速率下的波形,按照手册P16的要求,我检查了I2C的data setup time,这个时间远大于300ns, data  hold time时间为350ns,

400khz----data hold time

400khz---data setup time