This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
目前 dlpa3005 的VOFS VBIAS VRST,电压都正常,INTZ 和RESET_Z都为高电平,各个低压值都正常,从机dlpc3439的HOST_IRQ上电拉高后几秒后拉低,初始化成功,但是主机dlpc3439的HOST_IRQ一直为高电平;ILLUM_SW也没有电压,只有1V的左右。
问:1.LED_ANODE提供给LED的电源如何才能有?
2.主机dlpc3439的HOST_IRQ一直为低,其他信号都在正常,还有哪些地方会造成初始化失败?
DLPC3479对应的DMD型号是DLP4710LC,主要用于非显示领域例如3D打印,机器视觉等。DLPC3439对应的是DLP4710A,用于微型投影。如果系统初始化出错了,建议从这几个方面检查:DLPC3439和DMD的芯片供电,SPI flash是否烧录了正确的固件,DLPC是否有读flash,DMD的LS总线通讯是否正常。如果是PAD3005有异常,重点查一下外围电路是否正常,负载是否短路等。