This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLP4710EVM-LC: 使用官方给的DLPC-API-1.10示例工程,怎么将工程环境改为x64-release

Part Number: DLP4710EVM-LC


我在使用DLP4710evm-lc时,需要将通信环境改为x64-release版本,但官方给的API中cyusbserial.dll只有debug版本的,于是我在USB Serial SDK网站上找到他的X64版本的dll,使用时候发现,cypress_i2c.c 会抛出“运行时检查失败 #2 - 变量‘DeviceInfo’周围的堆栈已损坏。” 来自函数 GetCyI2CHandle。之后根据网上方法将 CY_MAX_DEVICE_INTERFACE 增加1,来增加设备通信,这样才能通信上,但是这也有问题,用工程dlp347x_dual运行一遍后,设备就连接不上了,利用GUI查看,显示为connectde,powered off,绿色的按钮按下也关不了,这好像是固件被烧坏了,我通过GUI重烧固件可以解决。

我想问的是:如何将通讯环境改为X64-release版本的,是否有合适的cyusbserial.dll,或者我还需要对程序进行哪些修改。期待您的回答