This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLPA3000: 开机上电时PWR1的1.1V能正常输出,PWR2的1.8V不输出

Part Number: DLPA3000


你好

我参考EVM原理图设计的电路中,PROJ_ON上电后自动拉高。但是测得有的电路1.1V有输出,1.8V没有输出电压,电压为0V。这时拔下电源后马上再次通电,1.8V就可以正常输出了。如果拔下电源等待15秒左右,1.8V输出完全降为0V后再通电,1.8V又不能正常输出了。只有在断电后1.8V没有完全降为0V前再通电才能正常输出1.8V。

请问这种情况是否可以断定是DLPA3000芯片有故障?出这种问题的概率大概是50个电路中有一个有这个问题,什么原因可能导致这个问题的出现?

谢谢