This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLP4710: 不能把投影图案烧录到固件当中

Part Number: DLP4710
Other Parts Discussed in Thread: DLP4500,

1.DLP4710-LC pattern-sequence模式,使用这个模块做三维重建时,希望能够实现把投影图案烧录到固件里面,然后再投影时,可以通道软件接口来设定指定编号的图案(比如说我烧录了12张图片,我能通过软件接口控制投影第7张,这个功能再DLP4500上有)。

2.是否有hid-usb版本的通信接口,现在的通信接口,再使用过程中经常出现把固件损坏,然后需要重新烧录固件,并且当前的通信依赖只能再下x86下运行,是否能在x64环境下运行。另外,对linux支持如何。

3.如果pattern-sequence模式没有,是否有其他比较可行的解决方案。