This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLP4500: 烧录新firmware后无法连接至电脑

Part Number: DLP4500

烧录新pattern后连接电脑始终显示没有connected。DLP4500烧录过程正常,没有弹出像其他人一样的“unable to enter programming mode”。重新断电以及删除驱动都试过,无效。

连接电源可以正常投射pattern,但是就是无法用软件控制。换了GUI V4.0和GUI V3.1都不行。

另外:烧录用的.bin文件是用GUI V4.0制作的,但是烧录是用GUI V3.1,不知道是不是受这个的影响。

求问怎么解决?