TI E2E 英文论坛海量技术问答的中文版全新上线,可点击相关论坛查看,或在站内搜索 “参考译文” 获取。

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLPC350: 外触发模式控制异常

Part Number: DLPC350

我使用dlpc350遇到了一个触发问题,请各位工程师帮助。

我设置的投影序列为先从flash img 1 中加入若干1bit图,再从flash img 0中加入若干5bit图组成投影序列,触发源设置为External Positive。PatternPeriod设置为10ms.

然后我发现了一个问题,当我设置patternExposure为3ms,并且validate成功后,接入触发信号后出现一次能触发成功一次不能触发成功交替出现的这种现象。

然后我将patternExposure改为5ms以上时,触发又完全正常了。另外我又改为Interneltrigger模式也是完全正常的。

请问产生这种现象应该如何解决?