This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLPC3433: DLPC3433CZVB与DLPC3433ZVB

Part Number: DLPC3433


Hello

由于供应链问题,我们由原先的DLPC3433CZVB  更换为DLPC3433ZVB。

目前出现了以下情况,在DSI接入时,会出现概率性光机无显示。但是LED是亮的。不良在20%~30%左右。

也有出现花屏的情况。

采用相同的固件用老的板子,DLPC3433CZVB,无此现象。

想咨询下,会是什么原因?DLPC3433ZVB是否有优化的空间?