This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLPA3005: DLPA3005外置开关电源没有电压问题

Part Number: DLPA3005
Other Parts Discussed in Thread: DLPC3479

我们的光机系统使用DLPA3005+DLPC3479+4710,上电后,3005电源电压1.1V、1.8V正常,偏压-14V、10V、18V正常。但是3005供给LED灯的外置开关电源,上桥臂G极电压是恒压1V,下桥臂为恒压0V,输出电压1V。正常情况下,上下桥臂有PWM波形,输出电压为3V。请问为什么?是3479和3005通讯异常吗?3005的82脚比较器参考电压是用来做什么的?这个82引脚需要3479控制吗?