This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLPC120-Q1: 请问Bezel offset命令的作用

Part Number: DLPC120-Q1


您好,

我在文档"PICCOLO SPI COMMAND INTERFACE DOC_NUM 2512380 Rev F – October 2014"里4.6节读到Bezel Offset (28h),

我理解为这个命令是用来将矩形图像在显示范围内做水平或竖直方式的整体偏移。

请问这个理解对吗?我用工具发送此命令图像并没有随之移动。请问如何正确操作并执行?

急等回复,感谢回答!